Choice: On | Off
Default: Off
Check (On) or clear (Off) to set the channel state.
Range:
0 to 7 (Normal Cyclic Prefix)
0 to 3 (Extended Cyclic Prefix)
The software assigns a Sequence Index number to each available sequence in the Group.
PHICH Transmission Configuration is showing PHICH Sequence Index in the PHICH group. The relationship between Sequence Index and orthogonal sequence is shown in the table below:
Choice: On | Off
Default: On
Check (On) or clear (Off) to set the coupling state.
When is turned on, the configuration for Subframe 0 is applied to all subframes in the sequence.
To configure each subframe in a sequence individually, turn off.
Use the
Data Source
Selection
dialog box to select , ,or
for the selected subframe.
= positive acknowledgement for the selected subframe.
= negative acknowledgement for the selected subframe.
= discontinuous transmission for the selected subframe.